AXIS#.PROFINET.SUPPSETPOINTDATA

Description

This command can be used to read the cyclic data sent from the controller to the drive in the configured supplemental telegram. Each index reads a 16-bit word in network byte order.

Example

-->AXIS1.PROFINET.SUPPSETPOINTDATA

[0] 4

[1] 0

[2] 160

[3] 0

[4] 0

[5] 0

[6] 0

[7] 0

-->AXIS1.PROFINET.SUPPSETPOINTDATA 0

4

Versions

Action Version Notes
Implemented 02-04-06-000  

General Information

Type Read Only
Units

N/A

Range 0 to 65535
Default Value N/A
Data Type Integer
Stored in Non-Volatile Memory No

Variants Supported

PROFINET drives: AKD2G-SPP

Fieldbus Information

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PROFINET.SUPPSETPOINTDATA

5225

Unsigned16[8]

Read Only

-